sew-eurodrive.com

Login
 
You are here: Home > News Overview > News
News
24.07.2007
PROFINET IO with PROFISAFE for MOVIFIT® now available
 
News
PROFINET IO with PROFISAFE

Mechanical protection devices, such as covers, barriers, or enclosures have so far been installed to ensure operator safety. Although these measures protected the employees during maintenance or changeover in the isolated work areas, it also inevitably meant that plant operation had to be stopped. More flexible and economic solutions had to be found to allow employees to work in safety areas and to ensure system operation.

 

SEW-EURODRIVE provides integrated safety technology for the decentralized MOVIFIT® drive control to meet these requirements. PROFINET/ PROFISAFE offers the user safety technology in combination with a future-oriented fieldbus system. The big advantage of this technology is that users do not need a separate safety controller and cabling. The PROFISAFE functionality is integrated in MOVIFIT®as option with the designation S11.

 

Features

 


More information on MOVIFIT®