With more than a million pumps sold, Watson-Marlow MasoSine, which is part of the Watson Marlow Pump Group, is one of the largest pump manufacturers worldwide. It is therefore a special honor for SEW-EURODRIVE to receive the Supplier of the Year award.
Click here to read the relevant press release in German language.
The photo shows (from left to right): Karlheinz Baader, SEW-EURODRIVE, Uwe Filsinger, SEW-EURODRIVE, Wolfgang Currle, SEW-EURODRIVE, Achim Bretzger, WATSON-MARLOW, Thomas Schmidt, WATSO-MARLOW, Jörg Jahn, SEW-EURODRIVE.
|