SEW-EURODRIVE is the first drive manufacturer to have a combination of efficient gear unit, motor and frequency inverter certified
according to the TÜV SÜD standard "Energy-Efficient Plant Technology":
the mechatronic MOVIGEAR® drive system. This offers customers an additional point of orientation for the selection of an energy-efficient drive unit.
The outstanding energy efficiency properties of the MOVIGEAR® system and the resulting saving potentials are now also substantiated by a new function of the SEW Workbench project planning
tool: the energy consumption analysis.
The "energy report" generated during this analysis, which is certified by TÜV SÜD, shows the total energy consumption for
the specific application and the configured drive train and forms the basis for selecting the most energy-efficient drive
technology.