SEW-EURODRIVE publishes a new volume of the series "Drive Engineering - Practical Implementation" named "Efficient plant automation with mechatronic drive solutions".
This publication refers to current questions, application requirements and trends to lead towards the optimal, efficient mechatronic drive solution. The starting point always is the actual situation and the requirements of the customer, who benefits from the experience SEW-EURODRIVE has gained from numerous successfully implemented projects.
This new publication is intended for plant manufacturers and operators who use decentralized plant automation for horizontal or vertical conveyor applications and the area in front of machines.
The publication is available in German and English and can be downloaded in section Documentation\Software\CAD. |