|
With the DriveBenefits portfolio, SEW-EURODRIVE generates measurable advantages for business partners in addition to just
delivering products. DriveTag, the new DriveBenefits module, supports the customers of SEW-EURODRIVE in handling material
flow and startup tasks. DriveTags are functional labels with bar codes printed on them. These labels are attached to drives or pieces of packages.
They contain important data for identifying the drive or package, such as order number or customer material number.
This identification makes it easier for customers to quickly identify deliveries using reading devices. In this way, precious
time is saved, the error rate in the reception of goods is reduced, and the material flow can be improved.
Advantages of DriveTag at a glance:
• Quick and efficient identification of the drive • Error prevention through automated processes • Saving of time in the goods receiving area and the in-house material flow
Customers can choose between various individually prepared drive labels or a packing piece label. Additional advantage: Customers
can specify their material designation or part number in the DriveConfigurator selection tool already during the engineering
process.
The data will be adopted automatically in the subsequent process steps or during electronic order processing.
More information about DriveBenefits
|