|
Motion control
|
With simple operation and a variety
of preset function blocks, the controllers allow for the efficient
implementation of motion functions, particularly when several axes
are to be coordinated. Since the axes are connected to a fast synchronous
system bus, all the motion control tasks can be taken over by one
controller.
|
|
Modular
|
In practice it is favorable in
many cases that I/Os, which directly depend on the motion sequence
or have an effect on them, are processed in the controller, for
example in the form of cam switches or touch probe events. In addition
to motion control, the controller then controls individual sequences
of sub-processes and automates a self-sufficient module of a machine.
Benefits: Less workload for the PLC, reduced response times, and
increased performance. Further, integrating functionality in the
controller can protect the company's know-how and reduce the workload
when changing the central automation system.
|
|
Stand-alone
|
Moreover, in conjunction with
the Drive Operator Panels (DOP) and the I/O system, all the components
required for an automation solution are provided – a drive with
suitable drive electronics, a control with a flexible I/O system,
as well as visualization. The stand-alone controller takes over
all the automation tasks ranging from motion control to sequence
control.
|
![]() |
Function blocks: Versatile
combinations and flexible use
Direct access to blocks
that allow for a certain drive function provide the highest level
of flexibility. The function blocks are clearly arranged in libraries
according to their functions and inverter type. With some experience,
users can flexibly combine these function blocks to create the optimum
program.
|
![]() |
Program modules: Optimally
combined for efficient use
The program modules comprise
bundled comprehensive drive functions. These can be simple functions
such as positioning, referencing or speed control, technology functions
for controlling a cam or synchronous operation, or functions for
multi-axis interpolations of kinematics. Once these program modules
have been integrated, the user merely has to concentrate on programming
the most important processes of the respective application. The
program modules provide the entire drive functionality via an interface.
This makes the program modules ideal for PLC programmers who want
to reduce the programming effort of the drive functionality.
|
![]() |
Libraries:
In
addition to a library for standard IEC functions, the MOVI-PLC® provides a library with
function blocks with suitable drive functions for each type of inverter
to allow for efficient programming. They comprise the following
functions: Enabling the drive, presetting the speed, positioning,
referencing, as well as reading or writing parameters.
In
addition, there are libraries for technology functions such as synchronous
operation, cam, virtual master axis, and cam control. These function
modules can be combined easily to create individual, tailor-made
solutions.
|
|
The following technology
options are available:
|
|
|
MPLCTecGearMotion
|
|
|
MPLCTecCamMotion
|
|
|
MPLCTecVirtualEncoder
|
|
|
MPLCTecCamSwitch
|
|
| back to top |